The Noise Figure Adjustment is used to adjust the network analyzer noise gain and noise power flatness.
The procedures for this adjustment may be found in the PNA on-line help. To find the procedures, perform the following steps:
On the PNA front panel, press the green Help button located in the Command block of keys. The on-line Help window is displayed.
The Help window may not be expanded fully. If the Hide icon is located in the upper left -hand corner of the tool bar, the help window is already expanded. Proceed to step 3. If the Show icon is in the upper-left corner, click it to expand the window.
From the left pane of the Help window, click the Index tab and type adjustment under Keywords, and click Display.
Double-click Adjustment Overview from the Topics Found window.
Double-click Noise Figure Adjustment to find the description and procedure.
This procedure may require up to 15-30 minutes.