N9933B/34B/35B/36B/37B/38B (N9938B requires Option 100)
The CalReady feature is the most basic measurement in Fieldfox. This test updates the CalReady default values as described in the Fieldfox datasheet. A simple S11 (and S22 for port 2) measurement is performed to verify that the defaults are appropriate.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
ECal Module, Type-N |
N4690D Options 0DC, M0F |
|
ECal Module, 3.5 mm
|
N4691D Options 0DC, M0F |
|
Short, Type-N (m) |
85054-60025 |
|
|
The following notes apply to illustrations in the FieldFox Help:
|