CalReady Refresh Functional Test

This test applies to the following models:

The CalReady feature is the most basic measurement in Fieldfox. This test updates the CalReady default values as described in the Fieldfox datasheet. A simple S11 (and S22 for port 2) measurement is performed to verify that the defaults are appropriate.

Required Test Equipment

Test Equipment

Recommended Model

Calibration kit, Type-N

85054B-H03

Calibration kit, 3.5 mm

  • For N9938A Option 100

85052D-H01

Connection Setups

The following notes apply to illustrations in the FieldFox Help:

  • Only a single representative model will be shown.
  • Some illustrations may differ than those in TME.
  • For procedures that apply to multiple ports, illustrations will show the setup on only one test port.

CalReady Refresh Test Setup