N9950A/51A/52A
|
|
Port 1 is always tested. Port 2 is only tested if Option 211 is installed. |
A source is used to provide a 10 dB power delta relative to 0 dBm at specific CW frequencies. This delta is measured by both the FieldFox receiver and a power meter. The difference between the two is considered to be the compression for the receiver at the given frequency.
This test requires the signal generator to have good repeatability. If repeatability is unacceptable, a warning message will be displayed.
|
Test type: |
functional |
|
Related specification: |
Receiver Compression (typical) |
|
Related adjustment: |
none |
|
Test Equipment |
Recommended Model Number |
|
Signal Generator #1
|
E8257D with options:
|
|
Signal Generator #1
|
N5183B Options [532 or 540], UNY |
|
Power Meter |
N1914A |
|
Power Sensor
|
N8482A |
|
Power Sensor |
N8485A-CFT |
|
Cable, Type-N |
11500C |
|
Cable, 3.5 mm (m) to 3.5 mm (m)
|
11500E |
|
Adapter, Type-N (f) to 2.4 mm (f) |
11903B |
|
|
The following notes apply to illustrations in the FieldFox Help:
|