|
|
This procedure is similar to, but completely separate from, the station calibration for the adjustments. The two station calibrations are based on different sets of frequency points. |
This process characterizes the test equipment used for most of the spectrum analyzer related tests. This station calibration is not required for all tests. The TME software will include this item on the test list when it is required.
After this station calibration is performed, it is intended that the test equipment remain undisturbed for the remainder of the tests. This refers to the additional test equipment for FieldFox analyzers with the SA Option 230/231 or Option 311. A station calibration expires after 24 hours.
The Station Calibration test is not listed in the test report because it does not perform measurements on the DUT. This test provides characterization of the power splitter. This characterization data is used in other tests.
|
Test Equipment |
Recommended Model Number |
|---|---|
|
Signal Generator #1 |
E8257D with options:
|
|
Attenuator/Switch Driver |
11713B Opt 001/024/060/101 |
|
Attenuator, 6 dB fixed |
8491A Opt 006 |
|
Attenuator, 1 dB step |
8494G Opt 001/024 |
|
Attenuator, 10 dB step |
8496G Opt 001/024 |
|
Power Meter |
N1914A |
|
Power Sensor |
E9304A Opt. H18 |
|
Power Splitter |
11667A |
|
Power Sensor Cable |
11730A |
|
BNC Cable |
8120-2582 |
|
Type-N Cable |
11500C |
|
Attenuator control cable |
8120-2703 |
|
|
The following notes apply to illustrations in the FieldFox Help:
|