|
|
|
This utility checks the validity of the factory calibration. The open/short/load calibration generates a set of reference corrections in the FieldFox. These corrections are stored in the “Factory Calibration” files. The “Corrected Measurement Uncertainty” graphs which appear in the datasheet rely on these reference corrections to be accurate.
This utility measures S11, and S22 of a calibrated short. If the factory corrections are appropriate, then the resulting S11/S22 measurement will be a flat trace. If the trace looks like a sinewave, then this suggests the correction doesn’t match the short used in the test. If the utility fails, then a new open/short/load calibration should be performed on the DUT.
|
Test Equipment |
Recommended Model Number1 |
|
Short, Type-N (m) |
85054-60025 |
|
Short, 3.5 mm (f) |
85052-60007 |
|
|
The following notes apply to illustrations in the FieldFox Help:
|