Source Isolation Utility

This test applies to the following models:

The purpose of this utility is to verify that the RF shielding is functioning properly following a repair.

This measurement is essentially two DANL measurements. The first step measures the DANL with the source off, and the second with the source on. The difference between the two DANL measurements is the source isolation. The test results are saved in a text output file. See the troubleshooting link below for information on accessing the text output file.

Related adjustment:

none

Required Test Equipment

Test Equipment

Recommended Model Number
(see main equipment list for alternative models)

Select from list below as per DUT connector type. Two required.

50 W Termination, Type-N

909A Opt 012

50 W Termination, 3.5 mm

909D Opt 011

50 W Termination, 2.4 mm

85138B

Adapter, Type-N (m) to 3.5 mm (m)

1250-1743

 

Connection Setups

The following notes apply to illustrations in the FieldFox Help:

  • Only a single representative model will be shown.
  • Some illustrations may differ than those in TME.
  • For procedures that apply to multiple ports, illustrations will show the setup on only one test port.

 

Source Isolation Utility Setup