This test verifies the frequency accuracy and range of the PNA's source output, and verifies the Test Port Output – CW Accuracy specification.
For single source PNAs, this test is only performed on Port 1, and the specification only applies to this port. For dual source PNAs, Port 3 is also tested. The process is the same as for Port 1. Approximately seven frequencies across the range of the RF PNA and up to 20 GHz on the microwave PNA are checked. Only frequencies up to 10 GHz are tested.
Power levels:
Microwave PNA = -17 dBm or higher
For troubleshooting help, see Frequency Accuracy Troubleshooting.
Below is the required test equipment for this test. Select the link that applies to your model.
Table A: PNA Type-N RF models:
E8356A, E8357A, E8358A
E8801A, E8802A, E8803A
N3381A, N3382A, N3383A
Table B: PNA 3.5 microwave models:
E8362A, E8362B, E8362C
Table C: PNA 3.5 mm & 1.85 mm microwave models:
|
PNA Type-N RF Models: E8356A, E8357A, E8358A |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter |
53230A Option 115 |
53131A/32A Options 010, 012, 124 53181A Options 010, 124 |
|
Adapter Type-N (f) to BNC (m) |
1250-1477 |
equivalent |
|
RF cable Type-N (m) to Type-N (m) |
N6314A |
8120-8862 |
|
BNC cable 1 |
any |
any |
|
Frequency Reference 2 |
internal |
house standard |
|
||
|
PNA 3.5 mm Microwave Analyzers: E8362A, E8362B, E8362C |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter |
53230A Option 115 |
53131A/32A Options 010 or 012, 124 53150A/51A/52A Option 001 53181A Options 010, 124 |
|
Adapter Type-N (m) to 3.5 mm (m) |
1250-1743 |
equivalent |
|
Adapter Type-N (f) to BNC (m) |
1250-1477 |
equivalent |
|
Adapter 3.5 mm (m) to 3.5 mm (m) |
1250-1478 |
83059A |
|
Adapter SMA (f) to BNC (m) |
1250-2015 |
equivalent |
|
Cable RF 3.5 mm (f) to 3.5 mm (f) |
85131-60013 |
85131-60010 |
|
BNC cable 1 |
any |
any |
|
Frequency Reference 2 |
internal |
house standard |
|
||
|
PNA Microwave Analyzers: |
||
|
2.4 mm: 1.85 mm: |
||
|
Test Equipment |
Recommended Model |
Alternate Model |
|
Frequency counter |
53230A Option 115 |
53131A/32A Options 010 or 012, 124 53150A/51A/52A Option 001 53181A Options 010, 124 |
|
Adapter Type-N (m) to 2.4 mm (m) |
11903A |
equivalent |
|
Adapter Type-N (f) to BNC (m) |
1250-1477 |
equivalent |
|
Adapter 3.5 mm (m) to 2.4 mm (m) |
11901A |
equvalent |
|
Adapter SMA (f) to BNC (m) |
1250-2015 |
equivalent |
|
Cable RF 2.4 mm (f) to 2.4 mm (f) or Cable RF 1.85 mm (f) to 1.85 mm (f) |
85133-60016 or N4697-60010 |
85133-60002
|
|
BNC cable 1 |
any |
any |
|
Frequency Reference 2 |
internal |
house standard |
|
||
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
The equipment list for this test includes a FreqReference1. It is indicated as optional because it may or may not require a separate piece of test equipment. The model for this equipment type may be FreqCounter1 Internal Ref or 10 MHz External Reference. When FreqCounter1 Internal Ref is specified, the frequency counter uses its internal frequency reference for its time base; a separate piece of equipment is not required. When 10 MHz External Reference is specified, an external 10 MHz reference is required to be connected to the counter (this will often be a house standard).
The calibration date, etc, for FreqCounter1 Internal Ref should match the frequency counter. The calibration information for 10 MHz External Reference will depend on the source used for the 10 MHz.
When 10 MHz External Reference is specified, the user must provide a value for frequency accuracy. Frequency Accuracy represents the worst case accuracy of the reference (maximum deviation from exactly 10 MHz) any time during the calibration period of the reference. The value is expressed in ppm and is entered via the Additional Properties key.
As an example, if the accuracy of an external frequency reference is +/- 1.0 Hz, then the accuracy is 1.0e-7. The value in ppm would be entered as 0.10.
If a separate counter is used as the 10 MHz External Reference instead of a house standard, here are some example frequency accuracy values:
|
Model |
Option |
Value |
|
53131A/32A |
no options |
8.6 ppm |
|
001 |
2.6 ppm |
|
|
010 |
0.1825 ppm |
|
|
53132A |
012 |
0.0385 ppm |
|
53181A |
no options |
8.6 ppm |
|
001 |
2.6 ppm |
|
|
010 |
0.1825 ppm |
|
|
53151A |
no options |
2.2 ppm |
|
001 |
0.183 ppm |
|
|
53230A |
no option |
1.7 ppm |
|
010 |
0.0155 ppm |
|
Note that values above 0.2 ppm will often give unsatisfactorily large measurement uncertainties.
Formula used to calculate the above values:
Frequency Accuracy = Time Base Error = (monthly aging rate * 12) + Temperature Stability