This test verifies that the power level is linear across the frequency range, and verifies the Power Sweep Range and Power Level Linearity specifications. It is performed at discrete frequencies and checks the linearity of the source over its automatic leveling control (ALC) range. It measures linearity across the specified power sweep range. The test does not check the linearity of any internal step attenuator.
For single source PNAs, this test is only performed on port 1; therefore the specification only applies to this port. For dual source analyzers, port 3 is also tested, and the process is the same as port 1. The port 2 PNA receiver is used to test port 1. The PNA receiver linearity is the standard against which the source linearity is checked.
The 20 dB attenuation during the test can come from one of two sources: the source internal step attenuator built into the PNA, or an external attenuation pad. When the internal step attenuator is used, it should be taken out of auto mode. (For the E8361A and E8362A 67 GHz PNAs, 10 dB is used in place of 20 dB.)
This test is performed using the Preset power level. For a list of PNA preset power levels, see the PNA Preset Power Level table located below the setup illustration.
For troubleshooting help, see Power Level Linearity Troubleshooting.
Below is the required test equipment separated by connector type. Select the link that applies to the connector type for your model.
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
|
Model |
Options |
Test Power Level |
|
All RF |
all |
0 dBm |
|
E8362A |
standard |
0 dBm |
|
UNL or 014 |
-5 dBm |
|
|
E8363A, E8363B |
standard |
-12 dBm |
|
UNL or 014 |
-17 dBm |
|
|
E8361A |
standard or 014 |
-15 dBm |
|
014 & UNL |
-17 dBm |
|