Source Power Accuracy Performance Test

This test confirms the accuracy of the PNA source output power across the frequency range of the PNA, and verifies the Test Port Output – Power Level Accuracy specification.

A separate test has been created for frequencies above 50 GHz to avoid unnecessary recalibration of the power sensors.

For single source PNAs, this test is only preformed on port 1. The specification only applies to this port. For dual source PNAs, port 3 is also tested. The process is the same for port 1. The test is performed at hundreds of CW frequencies across the frequency range of the PNA at the Preset power level. For a list of PNA preset power levels, see the PNA Preset Power Level table located below the setup illustration.

For troubleshooting help, see Power Level Accuracy Troubleshooting.

Required Test Equipment

Below is the required test equipment separated by connector type. Select the link that applies to the connector type for your model.

 

For Type-N Connector PNA Models

E8356A, E8357A, E8358A
E8801A, E8802A, E8803A
N3381A, N3382A, N3383A

Test Equipment

Recommended Model

Alternate Model

Power meter1

N1914A

E4419A/B
EPM-442A
N1912A

Power sensor

N8482A

8482A

Power sensor
(for > 3 GHz to 9 GHz models)
(not required when testing 3 GHz models)

N8481A

8481A

Power sensor cable
(Qty 2)
(1 required when testing 3 GHz models)

11730A

none

1. When testing PNAs that have a frequency range up to 3 GHz, the E4418A/B power meter can be used; therefore the E4412A power sensor and power sensor cable will not be required.

For 3.5 mm Connector PNA Models

E8362A, E8362B, E8362C

Test Equipment

Recommended Model

Alternate Model

Power meter

N1914A

E4419A/B
EPM-442A
N1912A

Power sensor

N8482A

8482A

Power sensor

N8485A

E9300A H25
8485A

Power sensor cable
(Qty 2)

11730A

equivalent

Adapter 3.5 mm (f) to 3.5 mm (f)

83059B

1250-1749

Adapter 3.5 mm (f) to Type-N (f)

1250-1745

equivalent

Adapter 3.5 mm (f) to Type-N (m)
(for power sensor calibration)

1250-1744

08485-60005

For 2.4 mm Connector PNA Models

E8363A, E8363B, E8363C
E8364A, E8364B, E8364C

Test Equipment

Recommended Model

Alternate Model

Power meter

N1914A

E4419A/B
EPM-442A
N1912A

Power sensor

N8482A

8482A

Power sensor

N8487A

8487A

Power sensor cable
(Qty 2)

11730A

equivalent

Adapter 2.4 mm (f) to 2.4 mm (f)

11900B

85058-60114
(1.85 version from cal kit)

Adapter 2.4 mm (f) to Type-N (f)

11903B

equivalent

Adapter 2.4 mm (f) to Type-N (m)
(for power sensor calibration)

11903D

08487-60001

For 1.85 mm Connector PNA Models

E8361A, E8361C

Test Equipment

Recommended Model

Alternate Model

Power meter

N1914A

E4419A/B
EPM-442A
N1912A

Power sensor

N8482A

8482A

Power sensor

N8487A

8487A

Power sensor

N8488A

V8486A with the V281A waveguide adapter1
(includes Option H67)2

Power sensor cable
(Qty 2)

11730A

equivalent

Adapter 2.4 mm (f) to 2.4 mm (f)

11900B

85058-60114
(1.85 version from cal kit)

Adapter 2.4 mm (f) to Type-N (f)

11903B

equivalent

Adapter 2.4 mm (f) to Type-N (m)
(for power sensor calibration)

11903D

08487-60001

  1. Combination of the V8486A power sensor and V281A adapter must be calibrated as a single unit—do not separate. For more information, click here.Closed
  2. Option H67 is an ANSI Z540-1 calibration for the V8486A power sensor with a V281A connector adapter (connected together).

 

Connection Setups

Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:

  • Only a single representative model will be shown.
  • Some illustrations may differ than those in TME.
  • For procedures that apply to multiple ports, illustrations will show the setup on only one test port.

Power Sensor Calibration Setup

Power Accuracy Measurement Setup

PNA Preset Power Level

Model

Options

Test Power Level

All RF

all

0 dBm

E8362A
E8362B
E8362C

standard

0 dBm

UNL or 014

-5 dBm

E8363A, E8363B
E8364A, E8364B

standard

-12 dBm

UNL or 014

-17 dBm

E8361A
E8361C

standard or 014

-15 dBm

014 & UNL

-17 dBm