This section lists the test equipment needed to run performance tests. Refer to each individual test for specific setup configurations with required cables and adapters. Not all of the listed test equipment needs to be connected to perform an individual test. To run a test, only the equipment specified for that test needs to be connected.
|
|
In all test equipment configurations, cables and adapters must be properly torqued. Exceeding recommended torque values can cause damage to a cable or adapter, and can cause inaccurate test results. |
| To make this connection | Use this driver or torque wrench and torque value | U2000A, U2000B,U2000H | U2001A,U2001B,U2001H | U2002A, U2002H | U2004A |
|
3.5 mm (m) to 3.5 mm (f) |
8710-1765 (8 lb-in, 5/16 inch open end) |
X |
X |
X |
X |
|
3.5 mm (m) to 3.5 mm (f) |
8710-1764 (8 lb-in, 20 mm open end) |
X |
|||
|
Type-N (m) to Type-N (f) |
8710-1766 (12 lb-in, 3/4 inch open end) |
X |
X |
X |
X |
|
|
|
|
Instrument |
Recommended |
Alternative |
|
Network Analyzer |
||
|
PNA Network Analyzer |
N5247B |
N5245A/AS E8361C |
|
ENA Network
Analyzer |
E5071C2 |
|
|
Calibration Kits |
||
|
50W Calibration Kit, Type-N for Network Analyzer |
85054B |
N4690B-M0F |
|
50W Calibration Kit, Type-N for Network Analyzer |
85032F |
|
|
50W Calibration Kit, 3.5 mm for Network Analyzer |
85052B |
N4691B-M0F |
|
Spectrum Analyzers |
||
|
Spectrum Analyzer |
E4440A Opt 1DS |
|
|
Signal Sources |
||
|
Signal Generator |
E8257D Opt 1E1 and (IEA or 1EU) and (532, 540, 550, or 567) |
|
|
Function Generator |
33622A |
33611A |
|
Power
Supply |
E3632A |
|
|
Power
Supply |
N5745A |
|
|
Power
Supply |
87422A |
|
|
Meters and Power Sensors (See below for calibration service ordering guidelines.) |
||
|
Power Meter6 |
N1914A |
N1912A |
|
Power
Sensor |
N8481A |
8481A 5 |
|
Power
Sensor |
N8481H |
8481H |
|
Power
Sensor |
E9304A |
|
|
Power
Sensor |
N8485A |
8485A |
|
Attenuators |
||
|
3 dB Fixed Attenuator |
8491B Option 003 |
|
|
6 dB Fixed Attenuator |
8491A Option 006 |
8491B Option 006 |
|
10 dB Fixed Attenuator |
8491B Option 010 |
8491A Option 010 |
|
10 dB Fixed Attenuator |
8493C Option 010 |
|
|
20 dB Fixed Attenuator |
8491A Option 020 |
8491B Opt 020 |
|
Power Splitters4 |
||
|
Splitter |
11667A |
|
|
Splitter |
11667B |
|
|
Miscellaneous Devices |
||
|
Directional Bridge |
86205A |
|
|
Directional Coupler (Power Accuracy Test of U2000/1/2H) |
Pulsar
Microwave |
|
|
Directional Coupler |
Werlatone C7926-10 |
|
|
Amplifier (Power Accuracy Test of U2000/1/2H) |
Mini
Circuit |
|
|
Amplifier |
Mini Circuit |
- |
|
Amplifier |
R&K Company Limited |
- |
|
Amplifier |
83020A |
- |
|
Filter |
RLC Electronics |
Low Pass Filter 0955-0306 and BNC (plug-m) to Type-N (f) 1250-1477 and BNC (jack-f) to Type-N (m) 1250-1476 |
|
Cables |
||
|
Type-N
(m to m) |
11500C |
|
|
BNC cable |
10503A |
BNC cable |
|
Wire (from power supply to amplifier) |
|
|
|
Adapters |
||
|
2.4 mm (f) to 3.5 mm (f) |
11901B |
|
|
2.4 mm (f) to Type-N (f) |
11903B |
|
|
Type-N (m) to 3.5 mm (f) |
1250-1744 |
|
|
2.4 mm (f) to Type-N (m) |
11903D |
|
|
Type-N (m) to BNC (m) |
1250-1473 |
|
|
2.4 mm (f) to 3.5 mm (m) |
11901D |
|
|
3.5 mm (f) to Type-N (m) |
08485-60005 |
|
|
Use the following guidelines to ensure power sensors used by the N7800A application receive the correct calibration service:
Order Option 1A7 when ordering new power sensors that will be used as working standards in N7800A TME calibrations.
Order the Keysight Cal + Measurement Uncertainty + GB calibration service for power sensor recalibration.
When ordering periodic calibration for instruments used as lab standards in the N7800A software, we recommend using “Keysight calibration + uncertainties” for power sensors, and “Keysight calibration + uncertainties + guardbanding” for all other items (please visit Selecting the Right Calibration Services). The N7800A software incorporates the ISO GUM Uncertainty in point-to-point uncertainty calculations. The special “H-series” calibration options in this table provide lower measurement uncertainties through use of direct comparison to devices directly characterized by NPL or NIST (or another NMI). Please order Option H99 to get electronic data for easy import into the N7800A (avoids manual entry). The overall resulting N7800A measurement uncertainties then reflects these lower device uncertainties. The equipment requirements of each N7800A calibration application are summarized in the specials calibration matrix which can be found at the Recommended Lab Standards and Special Cal Options website.
The Keysight Option H99 is a special option for the Roseville Service Center [only] which provides electronic calibration data available as a .csv file in TME N7800A format for all power sensors used with the N7800A TME application. N7800A TME is SSU calibration software used across Keysight SSU and by many self-maintainers. H99 must be requested from the Roseville SSU upon re-calibration only of any previously purchased power sensor and not for new purchases of BID Power Sensors. This option may be ordered in addition to any other required or requested Std Lab Calibration option (must also be ordered in addition to H99). Option H99 is recommended but not required.
|
|
The following models are not supported by Option H99:
|
To ensure data integrity for measurements carried out with Test Management Environment (TME), the following verification checks are carried out at the beginning of each test run. The checks are only performed on devices that require calibration data which directly affect the test results. If you are unable to meet the calibration requirements for these devices contributing to the measurement uncertainty only, you may still produce valid reports using the standard report format option which does not contain any measurement uncertainty information.
|
|
You are still required to enter calibration factors other than the default, but uncertainty related data is not required to produce standard format reports. |
The following table lists the standard checks performed by default:
|
Device |
Parameter Name and Description |
Limits |
A Failure Affects: |
| Power Sensor | CalFactor
(%)
The calibration factor, as a percentage |
Must be ≥10% and ≤150% at all points
Must not be 100% (the default) at all points |
All tests that require a power sensor |
| Uncertainty
(%)1
The uncertainty of the calibration factor, as a percentage |
Must be >0 and ≤10% at all points |
Tests that require a power sensor are also guard-banded by measurement uncertainty |
|
| Reflection
Coefficient Magnitude
The magnitude of the reflection coefficient |
Must be >0 and <0.5 at all points | Tests that require a power sensor are also guard-banded by measurement uncertainty | |
| Reflection
Coefficient Phase (Degree)
The phase of the reflection coefficient, as a degree |
Must be ≥–180° and ≤180° at all points
Must not be 0° (the default) at all points |
All tests that require a power sensor, except for Power Accuracy test | |
| Reflection
Coefficient Uncertainty
The uncertainty of the reflection coefficient magnitude |
Must be non-zero at all points | Tests that require a power sensor are also guard-banded by measurement uncertainty | |
| Reflection
Coefficient Phase Uncertainty(+/- Degree)
The uncertainty of the reflection coefficient phase, as a degree |
Must be >0° and ≤180° at all points | Tests that require a power sensor are also guard-banded by measurement | |
|
Power Splitter2 (Port 2) |
Source
Match
The magnitude of the equivalent source match |
Must be >0 and ≤ 0.5 at all points | All tests that require a power splitter |
| Source
Match Phase (Degree)
The phase of the equivalent source match, as a degree |
Must be ≥–180° and ≤180° at all points
Must not be 0° (the default) at all points |
All tests that require a power splitter | |
| Source
Match Uncertainty
The uncertainty of the equivalent source match magnitude |
Must be non-zero | Tests that require a power splitter are also guard-banded by measurement uncertainty | |
| Source Match
Phase Uncertainty (Degree)
The uncertainty of the equivalent source match phase, as a degree |
Must be >0 and ≤180° at all points | Tests that require a power splitter are also guard-banded by measurement uncertainty |
1) TME expects the power sensor calibration factor uncertainty to be absolute uncertainty.
2) The calibration data needed for power splitter is the Port 2 data. In the Calibration Factor test, the physical port of the power splitter with the Port 2 calibration data should be the test port which will be connected to Standard Power Sensor, Verification Power Sensor, or UUT.
|
|
Failure to comply with the Calibration Factor (%), Reflection Coefficient, Reflection Coefficient Phase (Degree), Source Match or Source Match Phase (Degree) limits will result in the test data being labeled Invalid in both the TME interface and any report format produced from the data. Failure to comply with the Cal Factor Uncertainty (%), Reflection Coefficient Uncertainty, Reflection Coefficient Phase Uncertainty (Degree), Source Match Uncertainty or Source Match Phase Uncertainty (Degree) limits will result in the data being labeled Invalid in the TME interface if Guard-banding is On, and in any report format, other than standard, produced from the data. If the Reflection Coefficient Phase Uncertainty (Degree) or Source Match Phase Uncertainty (Degree) is not available, please keep the default value ”0”. The application will calculate the worst case phase uncertainty and uses it to calculate the overall uncertainty. |
When running a test that required the calibration data, the test will check if all the required calibration data exists. If it is not, an error message will be prompted to ask you to enter the data.
Table 1 lists the UUT factory predefined frequency points at which the calibration data is required for the external test equipment (ETEs) for each UUT model.
Table 2 lists the equipments that need to be calibrated at the specific frequency points listed in Table 1.
Please have your ETEs calibrated at those frequency points and enter the calibration data in TME before you run any test.
| Frequency (GHz) | U2000A,U2000B, U2000H | U2001A,U2001B, U2001H | U2002A | U2002H | U2004A |
| 0.000009 | X | ||||
| 0.00003 | X | ||||
| 0.00005 | X | ||||
| 0.0001 |
X | ||||
| 0.0003 | X | ||||
| 0.0005 | X | ||||
| 0.001 | X | ||||
| 0.003 | X | ||||
| 0.005 | X | ||||
| 0.01 | X | X | X | ||
| 0.03 | X | X | X | ||
| 0.05 | X | X | X | X | X |
| 0.1 |
X | X | X | X | X |
| 0.3 | X | X | X | X | X |
| 0.5 | X | X | X | X | X |
| 0.8 | X | X | X | X | X |
| 1 | X | X | X | X | X |
| 1.2 | X | X | X | X | X |
| 1.5 | X | X | X | X | X |
| 2 | X | X | X | X | X |
| 3 | X | X | X | X | X |
| 4 | X | X | X | X | X |
| 5 | X | X | X | X | X |
| 6 | X | X | X | X | X |
| 7 | X | X | X | ||
| 8 | X | X | X | ||
| 9 | X | X | X | ||
| 10 | X | X | X | ||
| 11 | X | X | X | ||
| 12 |
X | X | X | ||
| 12.4 |
X | X | |||
| 13 |
X | X | X | ||
| 14 | X | X | X | ||
| 15 | X | X | X | ||
| 16 | X | X | X | ||
| 17 | X | X | X | ||
| 18 | X | X | X | ||
| 19 | X | X | |||
| 20 | X | X | |||
| 20.5 | X | ||||
| 21 | X | X | |||
| 21.5 | X | ||||
| 22 | X | X | |||
| 22.5 | X | ||||
| 23 | X | X | |||
| 23.5 | X | ||||
| 24 | X | X |
|
|
You can order the following option to calibrate the test equipment to meet the TME requirement on the test equipment's calibration data.
|
| Equipment type | Performance test | ||||
| VSWR | Power Accuracy | Calibration Factor | |||
| U2000A, U2001A,U2000B,U2001B, U2000H,U2001H | U2002A, U2002H | U2004A | |||
| StandardPowerSensor1 |
All UUT Model, 50 MHz only | + | + | + Range 2 |
|
| VerificationPowerSensor1 |
+ U2002A, U2002H |
+ | + | + Range 2 |
|
| StandardPowerSensor2 |
+ Range 1 |
||||
| VerificationPowerSensor2 |
+ All UUT Model except U2002A and U2002H |
+ Range 1 |
|||
| Splitter1 |
+ | + Range 2 |
|||
| Splitter2 |
+ Range 1 |
||||
| PowerSplitter1 3.5 mm F | + | ||||
+Refer to Table 1 for the required frequency points.
Range 1: 9 kHz to 50 MHz
Range 2: 50 MHz to 6 GHz
To enter the Device (power splitter or power sensor) calibration data into TME, follow these steps if electronic copy of the calibration data is available: