RF Output Path Insertion Loss

This test measures the insertion loss of the power sensor module RF Output cable. The intent of this test is to identify power sensor modules that have worn or damaged cables.

This test will perform an S21 measurement with the RF input port connected to port 1 and the RF output port connected to port 2. This test recalls the state saved in the Two Port Network Analyzer Calibration test.

Required Test Equipment

Test Equipment

Recommended Model Number

Option 504

N5532A/B and U5532C with

options 504 and

Z2092B-208

Option 518

Option 526

Option 550

PNA
Vector Network Analyzer

N5247B

 

X

X

X

X

ENA
Vector Network Analyzer

E5071C

X

 

 

 

 

50W Calibration Kit, Type-N

85054B

X

X

X

 

 

50W Calibration Kit, Type-N

85032F

X

X

 

 

 

50W Calibration Kit, 3.5 mm

85052B

 

 

 

X

 

50W Calibration Kit, 2.4 mm

85056A

 

 

 

 

X

E-Cal, Type-N

N4690D-M0F

 

X

X

 

 

E-Cal, 3.5 mm

N4691D-M0F

 

 

 

X

 

E-Cal, 2.4 mm

N4693D-M0F

 

 

 

 

X

Connection Setups

RF Output Path Insertion Loss Test Setup