This test measures the VSWR of the input port of the power sensor module with the RF output port terminated with a 50 Ohm load. This test recalls the state saved in the Two Port Network Analyzer Calibration test. A verification kit or a verification sensor can be used to verify the two port calibration.
The verification kit can be used instead of a power sensor to verify the network analyzer calibration. The software will only use one item in the verification kit to verify the cal. This item will be the largest fixed attenuator in the kit.
85055A — 50 dB attenuator
85053B — 40 dB attenuator
85057B — 40 dB attenuator
Each verification kit comes with the data needed to verify the network analyzer calibration.
In order to use the verification kit, save the .unc and .dat file for the largest fixed attenuator to following location depending on the operating system:
Windows 10:
C:ProgramData\Agilent Technologies\Test Management Environment\VerificationKit
|
|
For Windows 10, the VSWR test will create the path above if it is not found. You will have to access the destination folder by copying the compete path to Windows Explorer. |
You will need to rename the file by opening the
file and copying from the second line everything that follows #Part:
This number contains the model number and serial number of the fixed
attenuator. When mapping the verification kit in
TME, enter the five digit serial number located on the largest fixed
attenuator in the kit.
Copy the files
to C:ProgramData\Agilent Technologies\Test Management Environment\VerificationKit
Open the file and copy the part number.
Rename the files using the part number.
|
Test Equipment |
Recommended Model Number |
Option 504 |
N5532A/B and U5532C with |
Option 518 |
Option 526 |
Option 550 |
|
PNA |
N5247B |
|
X |
X |
X |
X |
|
ENA |
E5071C |
X |
|
|
|
|
|
50Ω Calibration Kit, Type-N |
85054B |
X |
X |
X |
|
|
|
50Ω Calibration Kit, Type-N |
85032F |
X |
X |
|
|
|
|
50Ω Calibration Kit, 3.5 mm |
85052B |
|
|
|
X |
|
|
50Ω Calibration Kit, 2.4 mm |
85056A |
|
|
|
|
X |
|
E-Cal, Type-N |
N4690D-M0F |
|
X |
X |
|
|
|
E-Cal, 3.5 mm |
N4691D-M0F |
|
|
|
X |
|
|
E-Cal, 2.4 mm |
N4693D-M0F |
|
|
|
|
X |
|
Power Sensor, Type-N, 18 GHz |
N8481A |
|
|
X |
|
|
|
Power Sensor, Type-N, 6 GHz |
N8482A |
X |
X |
|
|
|
|
Power Sensor, 2.4 mm, 50 GHz |
N8487A |
|
|
|
|
X |
|
Power Sensor, 3.5 mm, 26.5 GHz |
N8485A |
|
|
|
X |
|
|
Verification Kit, Type-N |
85055A |
X |
X |
X |
|
|
|
Verification Kit, 3.5 mm |
85053B |
|
|
|
X |
|
|
Verification Kit, 2.4 mm |
85057B |
|
|
|
|
X |
|
50Ω Termination, 3.5 mm |
902D |
X |
X |
X |
X |
|
|
50Ω Termination, 2.4 mm |
901D |
|
|
|
|
X |
OR