Calibrator Amplitude Adjustment

(Option PAA)

This adjustment adjusts the internal calibrator of the CXA-m PXIe signal analyzer for the full frequency range. The DAC is fixed at the maximum value, and the marker readout for the full frequency range is stored in the DUT's memory.

Required Test Equipment

None required.