In this process, a separate measurement is made at the RF output using a power meter, and based on the result, a computer algorithm calculates the value to adjust the output step attenuator.
|
Test Equipment |
Recommended Models |
|
Power meter |
N1914A |
|
Power sensor |
E9304A H20 |
|
Adapter, Type-N (f) to 3.5 mm (m) |
1250-1750 |
|
Frequency reference module |
M9300A |
Setup for Power Meter Calibration
Setup for Synthesizer Output Power