Setting the Primary VISA Library

To ensure Keysight VISA is the primary library, run the IOLS installer again. Then select modify, and then select Keysight VISA as primary VISA.

The installer will handle the file transfers in the system and IVI foundation folders which will be much easier for the user. Please note that this installation will overwrite NI’s version. Unless the application requires an earlier version, we recommend installing the latest version as it contains the latest fixes and features. For more information and to download Keysight IO Library, go to www.keysight.com/find/iosuite

To verify the installation, right-click the KCE icon in the taskbar and select About Keysight IO Control.