Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > AllocationCollection Class : Create Method


Glossary Item Box

Creates a new Allocation and appends it to the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Create() As Allocation
C# 
public abstract Allocation Create()
C++/CLI 
public:
abstract Allocation^ Create(); 

Return Value

If succeeds, returns handle to the new Allocation. If fails, returns null.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also