| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As Allocation _ ) As Boolean | |
| C# | |
|---|---|
public abstract bool Remove( Allocation item ) | |
| C++/CLI | |
|---|---|
public: abstract bool Remove( Allocation^ item ) | |
Parameters
- item
- Allocation to remove from the collection
Return Value
True, if the Allocation was removed from the collection. False otherwise.The minimum number of Allocation items is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)