| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub SetIQSymbolSequence( _ ByVal interleavedIQValues() As Single _ ) | |
| C# | |
|---|---|
public abstract void SetIQSymbolSequence( float[] interleavedIQValues ) | |
| C++/CLI | |
|---|---|
public: abstract void SetIQSymbolSequence( array<float>^ interleavedIQValues ) | |
Parameters
- interleavedIQValues
- interleaved real/imaginary pairs, one pair per symbol
| Exception | Description |
|---|---|
| System.ArgumentOutOfRangeException | Thrown if interleavedIQValues array is either empty, or unable to parse a valid float value at a specific location within the input array. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)