Keysight 89600 VSA .NET API
SetSymbolSubcarrierBlocks Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > Allocation Class : SetSymbolSubcarrierBlocks Method


value
An array where each element represents a SymbolSubcarrierBlock

Glossary Item Box

Sets the per-block mapping of active OFDM symbols and subcarriers for the current allocation.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetSymbolSubcarrierBlocks( _
   ByVal value As IReadOnlyList(Of SymbolSubcarrierBlock) _
) 
C# 
public virtual void SetSymbolSubcarrierBlocks( 
   IReadOnlyList<SymbolSubcarrierBlock> value
)
C++/CLI 
public:
virtual void SetSymbolSubcarrierBlocks( 
   IReadOnlyList<SymbolSubcarrierBlock^>^ value
) 

Parameters

value
An array where each element represents a SymbolSubcarrierBlock

Exceptions

ExceptionDescription
System.ArgumentException Thrown if an index is out of range for the current frame definition or otherwise invalid.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40

See Also