Keysight 89600 VSA .NET API
CustomModulationState Structure
Members  See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : CustomModulationState Structure


Glossary Item Box

This struct is for setting parameters for individual states within a custom modulation defined for use in Flex Frame modulation analysis.

Object Model

CustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState StructureCustomModulationState Structure

Syntax

Visual Basic (Declaration) 
Public Structure CustomModulationState 
   Inherits System.ValueType
C# 
public struct CustomModulationState : System.ValueType 
C++/CLI 
public value class CustomModulationState : public System.ValueType 

Remarks

The state represented here is a representation of an ideal symbol location for vector modulation. This type is immutable.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40

See Also