Gets or sets the frequency-domain FBMC filter coefficients.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property FrequencyDomainFilterCoefficients As Single() |
| C# | |
|---|
public abstract float[] FrequencyDomainFilterCoefficients {get; set;} |
Property Value
The default value is approximately [1.0, 0.972, 0.707, 0.235].
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 21.00
See Also