Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > FramePartCollection Class : Remove Method


item
FramePart to remove from the collection

Glossary Item Box

Removes the indicated FramePart from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As FramePart _
) As Boolean
C# 
public abstract bool Remove( 
   FramePart item
)
C++/CLI 
public:
abstract bool Remove( 
   FramePart^ item
) 

Parameters

item
FramePart to remove from the collection

Return Value

True, if the segment was removed from the collection.

Remarks

Note the first element in the collection cannot be removed.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also