| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property CdmGroupSymbolCount As Integer | |
| C# | |
|---|---|
public virtual int CdmGroupSymbolCount {get; set;} | |
Property Value
The default value is 1. The minimum is 1. The value can't be bigger than 1 if the pilot payload sequence is PayloadType.Unknown as we need to use reference pilots to despread the pilot in code domain. The value will be checked and coerced after Apply.This value is unitless.
This property is required for CDM (Code Domain Multiplex) overlapped MIMO pilot (or preamble) configurations. A value of N means that for each pilot (or preamble) subcarrier, the pilot (or preamble) values on N adjacent pilot (or preamble) symbols are used together to estimate the channel response, and this estimation result is applied to all the N adjacent pilot (or preamble) symbols.
This property along with CdmGroupSubcarrierCount decide the size of channel estimation CDM (Code Domain Multiplex) grouping unit in time domain and frequency domain.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00