Keysight 89600 VSA .NET API
InitialEqualizerMode Enumeration
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : InitialEqualizerMode Enumeration


Glossary Item Box

Mode of initial equalizer construction.

Syntax

Visual Basic (Declaration) 
Public Enum InitialEqualizerMode 
   Inherits System.Enum
C# 
public enum InitialEqualizerMode : System.Enum 
C++/CLI 
public enum class InitialEqualizerMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutomaticAutomatic selection of information for initial equalizer construction.—
ManualInformation in a specific symbol is used for initial equalizer construction.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

In Automatic mode the VSA tries to use any available information from known pilot and preamble subcarriers to estimate the initial channel equalizer. In Manual mode the user must specify which symbol index to use for constructing the initial channel equalizer. Symbol indexes start with 0 being the first symbol in the signal description. In both Automatic and Manual mode the equalizer is constructed using information from any known pilot and preamble subcarriers.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also