Gets or sets a value indicating the power threshold in dB relative to the max power of all available MIMO paths used for detecting whether an antenna port is active on an input channel for this PDSCH.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property AntennaDetectionThreshold As Double |
| C# | |
|---|
public virtual double AntennaDetectionThreshold {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double AntennaDetectionThreshold {
double get();
void set ( double value);
} |
Property Value
Default value is -36.0 dB.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.00
See Also