Keysight 89600 VSA .NET API
EqualizerSmoothingFilterLength Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : EqualizerSmoothingFilterLength Property


Glossary Item Box

Gets or sets the width, in subcarriers, of frequency-domain equalizer smoothing.

Syntax

Visual Basic (Declaration) 
Public Overridable Property EqualizerSmoothingFilterLength As Integer
C# 
public virtual int EqualizerSmoothingFilterLength {get; set;}
C++/CLI 
public:
virtual property int EqualizerSmoothingFilterLength {
   int get();
   void set (    int value);
}

Property Value

The default value is 40 subcarriers.

Remarks

This property is used only if EqualizerSmoothingMode is not EqualizerSmoothingMode.None.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also