Gets or sets the center frequency lock range.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property ExtendedFrequencyLockRangeWidth As Integer |
| C# | |
|---|
public abstract int ExtendedFrequencyLockRangeWidth {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int ExtendedFrequencyLockRangeWidth {
int get();
void set ( int value);
} |
Property Value
The default value is 10 subcarriers. The maximum value is equal to FftLength subcarriers, and the minimum is 1 subcarrier.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also