Gets an array of frame part IDs associated with each allocation ID, as listed in the
resource map.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Function GetFramePartIdPerAllocation() As Integer() |
| C# | |
|---|
public virtual int[] GetFramePartIdPerAllocation() |
| C++/CLI | |
|---|
public:
virtual array<int>^ GetFramePartIdPerAllocation(); |
Return Value
The array of frame part IDs associated with each allocation ID.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.00
See Also