Keysight 89600 VSA .NET API
GetPowerBoostLevelPerUser Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : GetPowerBoostLevelPerUser Method


Glossary Item Box

Gets the array of power boost levels for each user ID in the resource map.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetPowerBoostLevelPerUser() As Single()
C# 
public virtual float[] GetPowerBoostLevelPerUser()
C++/CLI 
public:
virtual array<float>^ GetPowerBoostLevelPerUser(); 

Return Value

The array of power boost levels for each user ID in the resource map.

Remarks

This property is an array of values, with one value for each user ID in the resource map array. The values are unitless. A value of 1 means no power boosting, while a value of 2 means there is a 6.02 dB power boost for the user ID. If this array is shorter than the highest user ID, any values past the end are assumed to be 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also