Keysight 89600 VSA .NET API
GetReferenceDataValues Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : GetReferenceDataValues Method


Glossary Item Box

Gets an array of reference data (refData) in-phase/quadrature (IQ) values.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetReferenceDataValues() As Single()
C# 
public virtual float[] GetReferenceDataValues()
C++/CLI 
public:
virtual array<float>^ GetReferenceDataValues(); 

Return Value

The array of reference data values (as IQ values).

Remarks

This is an array of values that indicate reference data (refData) in-phase/quadrature (IQ) values. Each reference data (refData) in-phase/quadrature (IQ) value of the subcarrier is represented by a complex in-phase/quadrature (IQ) value, real part first, then imaginary part.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also