Gets an array of symbol count per channel estimation CDM (Code Domain Multiplex) grouping unit for each user ID in the
resource map.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Function GetSymbolCountPerChannelEstimationUnitPerUser() As Integer() |
| C# | |
|---|
public virtual int[] GetSymbolCountPerChannelEstimationUnitPerUser() |
| C++/CLI | |
|---|
public:
virtual array<int>^ GetSymbolCountPerChannelEstimationUnitPerUser(); |
Return Value
An array of symbol count per channel estimation CDM (Code Domain Multiplex) grouping unit per user.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 27.40
See Also