Keysight 89600 VSA .NET API
IsDisplayEvmInPercent Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : IsDisplayEvmInPercent Property


Glossary Item Box

Gets or sets a value indicating whether EVM values are displayed as percentages.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsDisplayEvmInPercent As Boolean
C# 
public abstract bool IsDisplayEvmInPercent {get; set;}
C++/CLI 
public:
abstract property bool IsDisplayEvmInPercent {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When false, EVM values are displayed in dB. When true, EVM values are displayed with units of %.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also