| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsEqualizerUseData As Boolean | |
| C# | |
|---|---|
public abstract bool IsEqualizerUseData {get; set;} | |
Property Value
The default value is false.When set to true, data subcarriers are included when initializing ("training") the OFDM equalizer. Generally, if data subcarriers are included, pilot subcarriers should also be included.
Equalizer training uses all symbols in the ResultLength, not just those defined by MeasurementInterval and MeasurementOffset. This is so that the MeasurementInterval and MeasurementOffset can be changed to display parts of the signal, without also changing the equalizer.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)