| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsEqualizerUsePilots As Boolean | |
| C# | |
|---|---|
public abstract bool IsEqualizerUsePilots {get; set;} | |
Property Value
The default value is false.When set to true, pilot subcarriers are included when initializing ("training") the OFDM equalizer. This includes subcarriers marked as either Pilot or Unknown Pilot in the Resource Map.
Equalizer training uses all symbols in the ResultLength, not just those defined by MeasurementInterval and MeasurementOffset. This is so that the MeasurementInterval and MeasurementOffset can be changed to display parts of the signal, without also changing the equalizer.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)