| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsNormalized As Boolean | |
| C# | |
|---|---|
public abstract bool IsNormalized {get; set;} | |
Property Value
The default value is true.When true, IQ traces like IQ Meas, IQ Ref, and Error Vector are normalized so that the IQ Ref constellation points for non-boosted subcarriers have an RMS level of one (boosting will modify the RMS level of the constellation points). When false, the IQ traces are not normalized, so they have units of Volts.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)