Keysight 89600 VSA .NET API
IsPilotDefinedInTimeDomain Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : IsPilotDefinedInTimeDomain Property


Glossary Item Box

Gets or sets a value indicating whether the pilot is defined in time domain.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsPilotDefinedInTimeDomain As Boolean
C# 
public virtual bool IsPilotDefinedInTimeDomain {get; set;}
C++/CLI 
public:
virtual property bool IsPilotDefinedInTimeDomain {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also