Keysight 89600 VSA .NET API
IsPulseSearchThresholdAutomatic Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : IsPulseSearchThresholdAutomatic Property


Glossary Item Box

Gets or sets a value indicating whether the pulse search threshold is automatically determined.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPulseSearchThresholdAutomatic As Boolean
C# 
public abstract bool IsPulseSearchThresholdAutomatic {get; set;}
C++/CLI 
public:
abstract property bool IsPulseSearchThresholdAutomatic {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If false, the pulse search threshold is specified by the PulseSearchThreshold property. If true, the pulse search threshold is internally set to roughly -15 dB.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also