Keysight 89600 VSA .NET API
IsTrackAmplitude Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : IsTrackAmplitude Property


Glossary Item Box

Gets or sets a value indicating whether pilot tracking tracks the average pilot amplitude.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsTrackAmplitude As Boolean
C# 
public abstract bool IsTrackAmplitude {get; set;}
C++/CLI 
public:
abstract property bool IsTrackAmplitude {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If true, the average amplitude of the pilot subcarriers is tracked during pilot tracking. This means that the amplitude variation of the pilot subcarriers is backed out of all subcarriers before they are used. If there is amplitude droop in the signal, this will cause the droop to be removed and ignored by the measurement. However, if there is no amplitude droop, this could make the measurement slightly less accurate because the tracking may try to track pilot amplitude variation that is due to noise.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also