| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsTrackPhase As Boolean | |
| C# | |
|---|---|
public abstract bool IsTrackPhase {get; set;} | |
Property Value
The default value is true.If true, the average phase of the pilot subcarriers is tracked during pilot tracking. This means that phase variation of the pilot subcarriers is backed out of all subcarriers before they are used. This is normally needed for proper demodulation, to track frequency and phase drift in the signal.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)