Keysight 89600 VSA .NET API
ModulationScheme Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : ModulationScheme Property


Glossary Item Box

Gets or sets the modulation scheme for the analyzed signal.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ModulationScheme As ModulationScheme
C# 
public virtual ModulationScheme ModulationScheme {get; set;}
C++/CLI 
public:
virtual property ModulationScheme ModulationScheme {
   ModulationScheme get();
   void set (    ModulationScheme value);
}

Property Value

The default value is ModulationScheme.Ofdm.

Remarks

When set to ModulationScheme.FOfdm, the signal is assumed to be Filtered OFDM, and the properties in the FOfdm subclass can be used to control the demodulation. When set to ModulationScheme.Fbmc, the signal is assumed to use Filter Bank Multi-Carrier (FBMC) modulation, and the properties in the FbmcSettings subclass can be used to control the demodulation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also