| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property NamePerUser As String | |
| C# | |
|---|---|
public virtual string NamePerUser {get; set;} | |
Property Value
The default value is an empty string (which means that all user names are constructed automatically).This property is a comma-separated list of names, with one name for each user ID in the ResourceMap array. Backslash can be used to "escape" a comma character, and two backslashes in a row can be used to include a backslash character. If the number of names in the list is less than the highest user ID, names for the rest of the users are constructed automatically like "User0", "User1", etc.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00