Keysight 89600 VSA .NET API
PerUserStreamResultsEnabled Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : PerUserStreamResultsEnabled Property


Glossary Item Box

Gets or sets a value indicating whether per user ID active port stream results are included within OFDM Data Burst Info trace results.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PerUserStreamResultsEnabled As Boolean
C# 
public virtual bool PerUserStreamResultsEnabled {get; set;}
C++/CLI 
public:
virtual property bool PerUserStreamResultsEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

When true, per user ID active port stream results are included within OFDM Data Burst Info trace results. Otherwise per user ID active port stream results are not included within OFDM Data Burst Info trace results.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also