Keysight 89600 VSA .NET API
Preset Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : Preset Method


standard
The Standard to use for preset.

Glossary Item Box

Preset the CustomOfdm measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub Preset( _
   ByVal standard As Standard _
) 
C# 
public abstract void Preset( 
   Standard standard
)
C++/CLI 
public:
abstract void Preset( 
   Standard standard
) 

Parameters

standard
The Standard to use for preset.

Remarks

All properties are set to default values. In addition to the Custom OFDM measurement properties, this method also sets the measurement span to an appropriate value.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also