Keysight 89600 VSA .NET API
SetCdmGroupSubcarrierCountPerUser Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SetCdmGroupSubcarrierCountPerUser Method


cdmGroupSubcarrierCountPerUser
integer array, one value per user

Glossary Item Box

Sets an array of subcarrier count per channel estimation CDM (Code Domain Multiplex) grouping unit for each user ID in the resource map.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetCdmGroupSubcarrierCountPerUser( _
   ByVal ParamArray cdmGroupSubcarrierCountPerUser() As Integer _
) 
C# 
public virtual void SetCdmGroupSubcarrierCountPerUser( 
   params int[] cdmGroupSubcarrierCountPerUser
)
C++/CLI 
public:
virtual void SetCdmGroupSubcarrierCountPerUser( 
   ... array<int>^ cdmGroupSubcarrierCountPerUser
) 

Parameters

cdmGroupSubcarrierCountPerUser
integer array, one value per user

Remarks

This property is an array of values, with one value for each user ID in the ResourceMap array. The values are unitless. A value of N means that for each pilot (or preamble) symbol, the pilot (or preamble) values on N adjacent pilot (or preamble) subcarriers are used together to estimate the channel response, and this estimation result is applied to all the N adjacent pilot (or preamble) subcarriers on this symbol. If this array is shorter than the highest user ID, any values past the end are assumed to be 1. This method along with SetCdmGroupSymbolCountPerUser decide the size of channel estimation CDM (Code Domain Multiplex) grouping unit in time domain and frequency domain.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also