| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetCdmGroupSymbolCountPerFramePart( _ ByVal ParamArray value() As Integer _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetCdmGroupSymbolCountPerFramePart( ... array<int>^ value ) | |
Parameters
- value
- The array of symbol count per channel estimation CDM (Code Domain Multiplex) grouping unit.
This property is an array of values, with one value for each frame part ID, as listed in the per allocation frame part ID mappings array. The values are unitless. A value of N means that for each pilot (or preamble) subcarrier, the pilot (or preamble) values on N adjacent pilot (or preamble) symbols are used together to estimate the channel response, and this estimation result is applied to all the N adjacent pilot (or preamble) symbols on this subcarrier. This property along with SetCdmGroupSubcarrierCountPerFramePart decides the size of channel estimation CDM (Code Domain Multiplex) grouping unit in time domain and frequency domain. If this array is shorter than the highest frame part ID, any values past the end are assumed to be 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00