Keysight 89600 VSA .NET API
SetModulationPerAllocation Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MeasurementExtension Class : SetModulationPerAllocation Method


value
The array of QAM Identifiers associated with each allocation ID.

Glossary Item Box

Sets an array of QAM Identifiers associated with each allocation ID, as listed in the resource map.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub SetModulationPerAllocation( _
   ByVal ParamArray value() As Integer _
) 
C# 
public virtual void SetModulationPerAllocation( 
   params int[] value
)
C++/CLI 
public:
virtual void SetModulationPerAllocation( 
   ... array<int>^ value
) 

Parameters

value
The array of QAM Identifiers associated with each allocation ID.

Remarks

This property is an array of values, with one value for each allocation ID, as listed in the resource map array. The values are QAM Identifiers (indices into the modulation table). The actual modulation type (QAM Level) that each identifier maps to is defined by the QAM Identifier and QAM Level tables. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also