| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetPowerBoostLevelPerAllocation( _ ByVal ParamArray value() As Single _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetPowerBoostLevelPerAllocation( ... array<float>^ value ) | |
Parameters
- value
- The array of power boost level associated with each allocation ID.
This property is an array of values, with one value for each allocation ID, as listed in the resource map array. The values are unitless. A value of 1 means no power boosting, while a value of 2 means there is a 6.02 dB power boost for the user ID. If this array is shorter than the highest allocation ID, any values past the end are assumed to be 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00