| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetQamIdentifierPowerBoostLevels( _ ByVal ParamArray value() As Single _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetQamIdentifierPowerBoostLevels( ... array<float>^ value ) | |
Parameters
- value
- The array of power boost levels for each QAM Identifier.
This property is an array of values, with one value for each identifier in the QamIdentifiers array. The values are unitless. A value of 1 means no power boosting, while a value of 2 means there is a 6.02 dB power boost for the corresponding QAM identifier. If this array is shorter than the QamIdentifiers array, any values past the end are assumed to be 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00