| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetQamLevels( _ ByVal ParamArray value() As Integer _ ) | |
| C++/CLI | |
|---|---|
public: virtual void SetQamLevels( ... array<int>^ value ) | |
Parameters
- value
- The array of possible QAM constellation types.
This is an array of values that indicate QAM constellation types. Values in the QamIdentifiers array are indices into this QamLevels array. Valid values in this array are: 0 = Unknown, 1 = BPSK, 2 = QPSK, 3 = 8-PSK, 4 = 16-QAM, 5 = 32-QAM, 6 = 64-QAM, 7 = 128-QAM, 8 = 256-QAM, 9 = 512-QAM, 10 = 1024-QAM, 11 = 2048-QAM, 12 = 4096-QAM, 13 = 8192-QAM, 14 = 16384-QAM, 15 = 32768-QAM, 16 = 65536-QAM.
The value 0 means that the analyzer will attempt to auto-detect the actual modulation format by looking at statistics of the measured IQ values of the subcarriers that have been assigned this QAM level. Auto-detection is able to detect modulation formats that can't be directly specified in QamLevels, including BPSK-Q, BPSK+45, BPSK-45, QPSK+45, 4-PAM, 4-PAM-Q, 8-QAM, and 8-QAM+45. However, auto-detection is not able to detect 512-QAM, 1024-QAM, 2048-QAM, 4096-QAM, or above.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00